Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is ION Setup 3.x supported on Windows 10?
Product Line
ION Setup 3.0
ION Setup 3.1
ION Setup 3.2

Environment
Software Installation

Resolution
ION Setup 3.0 (Build 3.0.16218.01) and later versions are supported on Windows 10.

The latest version can be downloaded using the link below:
ION Setup Software

Note: ION Setup is still not UAC compliant. When installing ION Setup, log in with an Administrator account and right-click the installer to select "Run as Administrator".