Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
​Is Smoke Purge Option available on ATV660 Enclosed Drives?
Issue:
​Smoke Purge Option for the ATV660 Enclosed Drives

Product Line:
ATV660, Altivar 660

Environment:
All

Cause:
Smoke Purge option is not listed in Catalog

Resolution:
The Smoke Purge is available as an ETO (Engineered To Order) option.  Check with your local distributor if this option is necessary.