Issue:
Remote keypad that is used with the Altivar 320 AC Drive.
Product Line:
ATV320 drives
Environment:
Remote keypad
Cause:
Installation
Resolution:
Several remote keypad options are available.
Option 1
VW3A1101 Graphic Display Keypad
VW3A1102 Remote Mount Bezel, IP54 (or the VW3A1105 if not being mounted)
VW3A1103 Optional Cover/Door for Bezel (increases rating to IP65)
Option 2
VW3A1111 Graphic Display Keypad
VW3A1112 Remote Mount Kit IP65
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmware versions required:
ATV320- V2.9IE37
VW3A1111- V2.0IE51
Earlier versions are not compatible.
Option 3
VW3A1006 Remote Terminal Keypad, IP54
Option 4
VW3A1007 Remote Terminal Keypad, IP65
Then choose one cable to connect the remote keypad to the VFD:
VW3A1104R10 1 meter
VW3A1104R30 3 meter
VW3A1104R50 5 meter
VW3A1104R100 10 meter
Remote keypad that is used with the Altivar 320 AC Drive.
Product Line:
ATV320 drives
Environment:
Remote keypad
Cause:
Installation
Resolution:
Several remote keypad options are available.
Option 1
VW3A1101 Graphic Display Keypad
VW3A1102 Remote Mount Bezel, IP54 (or the VW3A1105 if not being mounted)
VW3A1103 Optional Cover/Door for Bezel (increases rating to IP65)
Option 2
VW3A1111 Graphic Display Keypad
VW3A1112 Remote Mount Kit IP65
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmware versions required:
ATV320- V2.9IE37
VW3A1111- V2.0IE51
Earlier versions are not compatible.
Option 3
VW3A1006 Remote Terminal Keypad, IP54
Option 4
VW3A1007 Remote Terminal Keypad, IP65
Then choose one cable to connect the remote keypad to the VFD:
VW3A1104R10 1 meter
VW3A1104R30 3 meter
VW3A1104R50 5 meter
VW3A1104R100 10 meter
Released for:Schneider Electric Nigeria