Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many simultaneous connections you can have with Vijeo Design'Air Plus?
Issue:
How many simultaneous connections you can have with Vijeo Design'Air Plus?

Product Line:
Vijeo Design'Air Plus, Vijeo Designer

Environment:
Remote access from Android/iOS phone/tablet to physical Human Machine Interface (HMI)

Resolution:
Vijeo Design'Air Plus from a single HMI only allows one connection at a time from a single phone or tablet.