How can we help you today?

How to create many LN with same DOs and DAs

User create the Data Model with many LN, and they had same DOs and DAs, there is a good way for it just need add DO and DA one time
1. Add LN in Data Model, take care, define a “Type A ”  for this LN
2. add DOs and DAs for this LN
3. If user want to add the same LN for different Instance, they just need add LN and choose the Type A for this LN.
4. be careful, if user change any DO or DA in these two LN, the other one will be changed.

Schneider Electric Nigeria