Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does my ATV6xx or ATV9xx trip on Overspeed (SOF) and measure very low output voltage, even at 60Hz?
Issue:
Overspeed Fault (SOF) on Process Drive

Product Line:
ATV600, ATV900

Environment:
Programming changes

Cause:
Programming change required

Resolution:
Need to program as follows or you will get Overspeed Fault and Measure very low voltage on the output of the drive, even at 60hz

How to run Process Drives with a Small or No Motor

1 - Set nPC (Motor Param Choice) to 'Mot Cosinus' [Main Menu] ->[Complete settings] -> [Motor parameters] -> [Motor data] -> [Data] -> [Motor Param Choice]


2 - Set Ctt [Motor Control Type] to 'U/F VC Quad' [Main Menu] -> [Complete settings] -> [Motor parameters] -> [Motor Control Type]

See overspeed faults attachment

3 - Set OPL to 'NO' [Main Menu] -> [Complete settings] -> [Error/Warning handling] -> [Output phase loss]

See Output Phase Loss Attachment


*See the applicable attached Programming Manual for further details.

Schneider Electric Nigeria

Attachment(s)
ATV600_Programming_Manual_EN_EAV64318_04.pdf [10.52 MB]
ATV900_Programming_Manual.pdf [11.83 MB]
Overspeed faults.png [77.07 KB]
Output Phase Loss Assign.png [212.27 KB]