Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Threshold at which the Altivar Process drive trips on SCF3 fault?
Issue:
SCF3 fault threshold at which the drive trips

Product Line:
ATV630, ATV650, ATV930, Altivar process

Environment:
All

Cause:
N/A

Resolution:
When the determined differential current of the three output phases is greater than
25% of the nominal inverter current, the inverter is switched off with fault message
"SCF3".