Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the SD card in the M340 CPU be accessed via the NOE or NOC using FTP
Issue
Can the SD card in the M340 CPU be accessed via the NOE or NOC using FTP

Product Line
M340

Environment
Windows 10

Resolution
The answer is no.

The SD card in the M340 CPU can only be accessed if you are directly connected to the CPU.