Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the ATV630 Flange mounting kit?

Issue:
Flange mounting kit part number for ATV630.

Product line:
ATV630, Altivar Process

Environment:
All models.

Resolution:
The flange mount kit is based on the ATV630 part number.  See the following spreadsheet for selection.

See attachment

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

Schneider Electric Nigeria

Attachment(s)
FA299185.jpg [107.38 KB]