Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATV600 series Drives compatible with Ethernet?
Issue:
ATV600 Ethernet Modbus TCP compatibility

Product Line:
Altivar Process Drives

Environment:
All

Cause:
Installation

Resolution
Yes, Ethernet TCP/Modbus TCP is standard integrated functionality. Ethernet IP requires a separate Option Card VW3A3720 (min. Firmware ver. 1.5) or (min. Firmware ver. 1.6) VW3A3721. These are both combination TCP/IP and Ehternet IP Option Modules with dual port daisychain functionality.