Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the TTL for a Quantum 140NOC78x00?
Issue
What is the TTL (Time To Live) for a Quantum 140NOC78x00?


Product Line
140NOC78000
140NOC78100


Resolution
For a Quantum 140NOC78x00 with firmware versions less than 1.70, the TTL (Time To Live) for Point to Point EIP communications through routers, is 1.

For a Quantum 140NOC78x00 with firmware versions equal to or greater than 1.70, the TTL (Time To Live) for Point to Point EIP communications through routers, is 64.

The TTL remains at 1 for Multicast EIP communications.

If a TTL greater than 1 is required for Point to Point EIP communications, then upgrade the 140NOC78x00 firmware to version 1.70 or higher.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings