Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How can you turn off the flashing red caution LED on the ATV630 and ATV930 process drives?
Issue:
Turning off the flashing red caution LED on the ATV630 and ATV930 process drives.

Product Line:
Altivar ATV630 and ATV930

Environment:
All

Cause:
There is a default alarm set in the warnings group for Analog input AI1, AI2, and AI3 that has to be turned off.

Resolution:
The warning LED is triggered when a Warning Group item is activated.  The factory default has many items selected for monitoring under Warning Group 1.  A typical warning is caused when an analog input is configured for 4-20mA, but the signal is not present.



From the Main menu:
  1. Scroll to Complete Settings and press OK
  2. Select Error Warning Handling and press OK
  3. Select Warnings Group Configuration and press OK
  4. Select Warn group 1 definition and press OK
  5. Now (almost halfway down the list) uncheck "AI1 4-20 Warning", "AI2 4-20 Warning", and "AI3 4- 20 Warning" boxes.


See attachment

Now the red flashing warning light will turn off.

Schneider Electric Nigeria

Attachment(s)
ATV630 Warning groups.png [52.65 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings