Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Why can't I connect to my Magelis HMI with Vijeo Design'air?
Issue:
Vijeo Design'Air shows a "connection refused" error.

Product Line:
Vijeo Designer 6.1, Vijeo Designer 6.2, Vijeo Design'Air

Resolution:
This error typically occurs if you have Vijeo Design'Air security setup in your HMI application. You must set _RemoteViewer.DisableConnections to 0 on the HMI side before the app can connect.

The following video demonstrates how to configure security settings in Vijeo Design'Air: