Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between an ATV930 part number and an ATV930 part number with "C" at the end?

Article available in these languages: Spanish

Issue:
Meaning of the C suffix on an ATV930.

Product Line:
ATV930 series

Environment:
All models, All serial numbers

Cause:
Feature clarification

Resolution:
The ATV930 series drives without the "C" on the end include an internal braking transistor.
If the part number has a "C" at the end, the braking transistor is not included.  To use a braking resistor, a separate braking unit must be purchased separately.