Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Removing Disk on Chip (DOC) from CM4000/3000 series meter
Issue:
User would like to know how to remove Disk on Chip (DOC) from Powerlogic CM4000/3000 series meter.

Product Line:
CM4000, CM3000 series meter

Resolution:
The video within this article provides user step-by-step procedure on how to remove Disk on Chip (DOC) from CM4/CM3 series meter.

NOTE: The document attached along this article describes how to install the Memory Expansion chip. However, the same document can be used as reference in order to remove the Disk on Chip from CM4/CM3 meter.

Schneider Electric Nigeria

Attachment(s)
Replace_DOC.pdf [790.5 KB]