Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the touch-up paint for the ATV630 Outdoor drive enclosure?

Issue:
Needs the part number of the touch-up paint for the ATV630 Outdoor drive

Product Line:
ATV630


Resolution:
Schneider does not have a part number for ordering touch-up paint. Recommending acquiring the paint from Orbittx. They offer spray cans and brush bottles. Our enclosures (both wall mount and floor standing) are standard RAL7035 color.
Orbittx website:
http://www.orbittx.com/index.php?option=com_content&view=article&id=48&Itemid=53

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)