Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the ATV320 be used for single phase input to run a three phase motor?

Article available in these languages: Spanish

Issue:
ATV320 single phase supply to a three phase motor

Product Line:
ATV320, Altivar 320 Machine drive

Environment:
All models

Cause:
Short circuit and HP ratings for VFDs supplied with single phase power.

Resolution:
Yes, the ATV320 is suitable for single phase supply to three phase motors.  See the information included in the Getting Started Annex, document NVE21777 attached to select.

Schneider Electric Nigeria

Attachment(s)
ATV320_Getting_Started_Annex_NVE21777_07.pdf [199.09 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings