Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I connect to a SoMachine controller via an EWON gateway?
1 - Setting up the eWON configuration through eCatcher


2 - Setting up the SoMachine controller via SoMachine to connect via the eWON gateway


In addition:
From SoMachine - Had him check Dial up via "Active path" under the Project Settings and communication.
From the Gateway Management Console under the Static Remote Connection - Added the local IP address of the SoMachine controller