Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Upon connecting the device in Ecoreach and changing the IP configuration to static in project area, I can’t see the IPV4 address, subnet etc. What could be wrong here?
My Ecoreach project is saved with DHCP configuration in Communication section of a device. But I have changed the communication configuration of IFE to static through the webpage.
A refresh button is given in Ecoreach device value area to refresh such parameters when a situation like this happens. Once you refresh, the values will be updated in the Device values column.