Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many MAC addresses does the M580 CPU have?

Issue
Number of MAC addresses on a M580 CPU

Product Line
M580 PAC

Environment
Unity Pro or Control Expert

Resolution
Each M580 CPU has 3 MAC Addresses. But only 1 MAC address, which is the Service port MAC address, is silk screened on the CPU Module and is associated with the Unity program assigned IP address.
The other MAC addresses are required for the other two physical Ethernet ports. Each physical Ethernet port is required to be assigned a unique MAC address.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings