Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the specifications on R1 and R2 Relays for ATV61 or ATV71 Drives?
Issue:
ATV61/ATV71 specifications on R1 and R2 Relays

Product Line:
ATV71, ATV61, Altivar 61, Altivar 71

Environment:
All

Cause:
NA

Resolution:
R1A  N/O contact
R1B  N/C contact
R1C  Common point C/O contact of programmable relay R1
R2A  N/O contact
R2C  Common Point C/O contact of programmable relay R2

• Minimum switching capacity: 3 mA for 24 Vdc
• Maximum switching capacity on resistive load:
5 A for 250 Vac or 30 Vdc
• Maximum switching current on inductive load (cos ϕ = 0.4 L/R = 7 ms):
2 A for 250 Vac or 30 Vdc
• Reaction time: 7 ms ± 0.5 ms
• Service life: 100,000 operations at max. switching power