Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Main Function for the Under voltage release coil (MN) installed inside NSX MCCB ?

MN undervoltage release

The MN release opens the circuit breaker when its supply voltage drops to a value below 35 % of its rated voltage Un.

Undervoltage tripping, combined with an emergency-off button, provides fail-safe tripping.

The MN release is continuously supplied, i.e. if supply is interrupted:

either voluntarily, by the emergency-off button,

or accidentally, through loss of power or faulty wiring,

the release provokes opening of the circuit breaker.