Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to log data under a specific device name instead of VIP.DEFAULT in Power Monitoring Expert

Issue
Is it possible to change the source name that logged data is associated with when setting up a Data Recorder Module, and have the historical data logged under any other device/node?

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Designer
ION Setup

Resolution

*When creating custom measurement labels, only use alphanumeric characters such as 1,2,3, a,b,c, and underscores.  Special characters such as !,#, or $ cannot be written to the SQL databases successfully and will cause System Log Events showing the text below:*
"Failed to write config info to the database because 'Could not add measurement map entry.'. Will retry in 60s."

Use this article for native PME measurement names: List of 'Official' Power Monitoring Expert Measurement Labels | Schneider Electric USA


When linking a source/module output to a Data Recorder Module, the naming convention below can be used to modify the source name that the logged data will be associated with.

"Measurement@Group.Device" ← note the use of the "@" symbol, as this technique is commonly referred to as "@ sign redirect"

This convention can be used with devices that are currently within the Management Console or to create a new virtual device that does not yet exist.

Example:

Step1)

Use the management console to find the group name and the device name of the meter that you would like to log the data from the VIP under
mc
In this example, the meter will have group name = Sub_1 and device name = Meter_1
Devices from the management console are stored in the database of the software in the following format → "GroupName.DeviceName"
Notice how the software condenses the group name and the device name together and adds a period in between them
=> Therefore, the format of the device in this example is Sub_1.Meter_1
Step 2)
Open Designer and use the two most commonly used modules for this procedure, the arithmetic module and the data recorder module.
*For more information on the modules in Designer and what they are capable of, please see the following online article: ION Reference | Schneider Electric
Right-click and edit the output of the arithmetic module using the @ sign redirect method to log the data that is being output by this module under the meter in this example, Sub_1.Meter_1
setup module
To edit the output register of this module, double-click the result; in this case, it is named Art11 Result1


The image below shows the scenario that will log the source value as the known measurement "kWh" under the device name "Sub_1.Meter_1".

An Arithmetic Module is used to link its output to a Data Recorder Module, as shown below:
register owners

It is important to note the device name, whether a physical meter or virtual, that comes after the @ symbol.  This will control the source that should be selected when either configuring a Data Log Viewer through Vista or running a Report through the web applications to view the historical data.

NOTE: Default measurement labels should be used when naming registers, as this will ensure compatibility with other PME features.
For a list of 'Official'  Power Monitoring Expert measurements and their naming convention, See article List of 'Official' Power Monitoring Expert Measurement Labels | Schneider Electric USA

Schneider Electric Nigeria

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: