Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the temperature limit conditions for the Altivar Process Drive (IP21)?
Issue:
Temperature limit conditions for the Altivar Process Drive (IP21).

Product Line:
Altivar 630 and Altivar 930 (IP21)

Environment:
All serial numbers for Altivar 630 and Altivar 930

Cause:
N/A

Resolution:
All “IP21 Products (except floor standing products) can be operated up to 50°C without de-rating and up to 60°C with de-rating.
The de-rating factor depends on the ambient temperature, the mounting position and the switching frequency (see applicable Installation Manual).