Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What type of MIB file Sepam SNMP implementation utilizes?
Sepam SNMP implementation utilizes the industry standard MIB2 which provides information about the ACE850 communication module. ACE module only supports MIB2 because the information it provides is pretty basic which is why it does not require any MIB file. Please see the attachment for the list of information being provided.

Schneider Electric Nigeria

Attachment(s)
Sepam SNMP Configuration.pdf [65.5 KB]