Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the displacement power factor on the ATV630 drive be better than the ATV61/ATV71 drives?
Issue:
Is the displacement power factor ratings on the ATV630 drive better than the ATV61/ATV71 drives?

Product Line:
ATV630

Environment:
All

Cause:
Is the power factor more efficient than an ATV 61 and ATV71 drive?

Resolution:
The displacement power factor for the ATV630 is similar to the ATV61.
See attachment for the current ATV630 and ATV930 displacement power factor ratings.

Schneider Electric Nigeria

Attachment(s)
Altivar Process DPF-PF_IE03draft.pdf-customer-inquiry.pdf [118.02 KB]