Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are general schematics available for the Altivar 660 Drives?
Issue:
ATV660 Drives schematics availability

Product Line:
Altivar 660 Systems Drives

Environment:
All model numbers, all serial numbers

Cause:
N/A

Resolution:
No, there are no general schematics/wiring diagrams available. Each drive has it own unique wiring because it is a custom enclosed package with multiple options.