Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what is the rated Current For the Contactor LC1D09 if it works on AC1 Loads ?
The rated current for the contactor LC1D09 on 380 V AC if works with loads of type AC1 is 20 A