Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Modicon M241 support Ethernet/IP as a scanner device?
Issue:
Does the Modicon M241 support Ethernet/IP as a scanner device?

Product Line:
Modicon M241 PLC, SoMachine / EcoStruxure Machine Expert software

Environment:
PLC Communication Ethernet Protocol

Resolution:
Only the TM241CE24x or TM241CE40x controllers will support Ethernet/IP (EIP) as a TCP scanner.
This requires SoMachine v4.2 configuration software or higher, or EcoStruxure Machine Expert software (all versions).