Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are some of the benefits to an active front end in comparison to a classic approach front end with the Altivar 680/980 Series Variable Frequency Drives?
Issue:
Altivar 680/980 Series drives active front end benefits in comparison to a classic approach front end:
  • 12 pulse input
  • 18 pulse input
  • 6 pulse input with Harmonic filter

Environment:
All

Cause:
Harmonics

Resolution:
An active front end with the Altivar 680/980 Series Variable Frequency Drives provides a reduced foot-print size, higher efficiency standards and reduced EMI.