Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do any Altivar Drives meet IEEE 519 requirements?
Issue:
Altivar Drives with IEEE 519 specifications.

Product Line:
Altivar 680, ATV680 Active Front End

Environment:
Known Harmonics Issues

Cause:
All

Resolution:
The ATV680 product line with active front end built in will meet requriements to fall within the IEEE 519 System Specification.
This is documented on page 13 of the ATV680 Low Harmonic Drive Systems Handbook (attached).

Schneider Electric Nigeria

Attachment(s)
ATV680_Handbook_EN_NHA37113_02.pdf [7.46 MB]