Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What terminal do you use for run status and fault status?
Issue:
Run status and fault status terminals.

Product Line:
ATS22

Environment:
All

Cause:
Run status and fault status terminations

Resolution:
For run status they are wired to terminals 52 & 53
For fault status they they are wired to 40 & 41