How can we help you today?

How do I test a Hot Standby PLC that is going to be a standalone system with I/O drop configured if the drop is not present?

Issue
How do I test a Hot Standby PLC that is going to be a standalone system with I/O drop configured if the drop is not present?

Product Line
EcoStruxure Control Expert, Modicon Quantum

Environment
140CPU67160, Control Expert v15.0


Resolution
A standalone Hot Standby PLC with a drop configured but not present will come up in Run Offline mode. In order to boot in Online set %S84 to 1.

Schneider Electric Nigeria
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings