Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the Ethernet Multi-link option card used on the Process drives?
Issue:
Ethernet IP/ Modbus TCP Multi-Drive Link Communication Module part number.

Product Line:
ATV630

Environment:
All

Cause:
Ethernet IP/ Modbus TCP Multi-Drive Link Communication module

Resolution:
Part number is VW3A3721. This card will only work on ATV630 drive version 1.6IE12 version or higher.
photo A
https://www.se.com/us/en/product/VW3A3721/ethernet-ip,-modbustcp,-multidrive-link-communication-module---2rj-45/

This card is not needed on the ATV930 series drives. Multi-link is built in.

Schneider Electric Nigeria

Attachment(s)
Altivar Process ATV600_VW3A3721 (2).pdf [88.84 KB]