Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What fuse is needed to be used with Com'X 200/210/510?
Product Line
Com'X 200 (EBX200)
Com'X 210 (EBX210)
Com'X 510 (EBX510)

Environment
Fuse protection type

Resolution
  • 100-230 V AC option (Com'X 200 only)
    • Fuse protection type T 0.63AE/250V (F1)
  • 24 V DC option
    • Fuse protection type 3.15AL/250V (F1500)
  • Power Over Ethernet (PoE)
    • No fuse needed