Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which HMIs can be programmed with EcoStruxure Operator Terminal Expert Basic?
Issue
Which HMIs can be programmed with EcoStruxure Operator Terminal Expert Basic / Vijeo XD Express?

Product Line
EcoStruxure Operator Terminal Expert (previously named Vijeo XD)

Environment
Configuration software on Windows PC

Resolution
In EcoStruxure Operator Terminal Expert v3.1 and v3.2 Basic License, the following Magelis HMI can be programmed:
HMISTO7 Series: HMISTO705, HMISTO715, HMISTO735
HMIST6 Series: HMIST6200, HMIST6400, HMIST6500, HMIST6600, HMIST6700

In the previous version, Vijeo XD v3.0 Express License, the following Magelis HMI can be programmed (as the HMIST6 series did not exist yet):
HMISTO705, HMISTO715 and HMISTO735