Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M340, Premium – Rack extension – Maximum length
Issue

While using M340 extension rack and cables, Is the maximum distance between racks is 12 m while the total cumulative length is 30m?

Product Line

M340, Premium


Issue

The documentation "35012676_K01000-02.pdf" is not ambiguous:
  • 4 racks maximum
  • Maximum length of 30 meters (this is the maximum cumulative length between the racks)
The different cables proposed are compatible with the above requirements.


If a customer use only 2 racks, he can realize a custom cable, but with a maximal length of 30 meters.