Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum motor cable length for ATV660 drives?
Issue:
Is there a recommendation for the maximum motor cable length for ATV660 drives?

Product line:
Altivar ATV660

Environment:
All

Cause:
N/A

Resolution:
150 meters with shielded cable
250 meters with unshielded cable

300 meters with shielded cable and option "300m DV/DT filter"
500 meters with unshielded cable and option "300m DV/DT filter"

Schneider Electric Nigeria

Attachment(s)
ATV660_Handbook_EN_NHA37111_02 cable length.pdf [140.3 KB]