Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Looking to replace the LXM23DU04M3X and BCH0602O12A1C
Issue:
Looking to replace the LXM23DU04M3X and BCH0602O12A1C servo motor

Product Line:
LXM23

Resolution:

The direct replacement is:
LXM28AU04M3X and BCH2LD0431CA5C combination:
- Supply voltage single phase 200/240 VAC or 3 phase 200/240 VAC, 50/ 60 Hz
- Nominal torque 1.27 Nm
- Maximum peak torque 3.81 Nm
- Nominal speed 3000 RPM
- 0.4 Kw motor rating
- 0.27 kgcm2 motor inertia without holding brake
You cannot copy the parameters from the old drive to the new drive. They will have to be entered manually in the new LXM28 drive.