Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the ATV630 ABS rated?
Issue:
Are the ATV630 ABS rated?

Product Line:
ATV603, ATV930

Environment:
ABS Rating

Cause:
n/a

Resolution:
The ATV630 and 930 drives are in process of ABS certification. This is expected to be achieved in very near future.