Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to undock the outout window to allow a obtain more workspace.
Issue
How to undock the outout window to allow a obtain more workspace.

Product Line
Unity

Environment
Windows 10

Resolution
The following steps can be used to undock the output window to obtain a larger workspace by
  • Start Unity
  • Open an application
  • Right click on one of the tabs in the output window.

tr

  • Click on 'Allow Docking'.
fhgjkl;

This causes the ouput window is resized to a smaller window that floats on top of Unity and it can be moved out of the way.
This gives the user more space to work with the application.