Issue:
ATV320 Unable to change the logic inputs in the I/O menu.
Product Line:
ATV320
Environment:
All
Cause:
Programming logic inputs
Resolution:
You can not assign a function to the logic inputs in I/O menu.
Those are read only parameters.
You must assign a logic input to the function you need.
Example, If you want to assign freewheel stop to LI2, you would need to go to CONF / FULL / FUN / STT, then go to NST and assign LI2 to NST.
ATV320 Unable to change the logic inputs in the I/O menu.
Product Line:
ATV320
Environment:
All
Cause:
Programming logic inputs
Resolution:
You can not assign a function to the logic inputs in I/O menu.
Those are read only parameters.
You must assign a logic input to the function you need.
Example, If you want to assign freewheel stop to LI2, you would need to go to CONF / FULL / FUN / STT, then go to NST and assign LI2 to NST.
Released for: Schneider Electric Nigeria