{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to setup an ATV630 and ATV930 with catch on the fly function?
Issue:
How to add the catch on the fly feature to an ATV630 and ATV930

Product line:
Altivar Process 630 and 930

Cause:
Catch on the fly detects a spinning load and picks up control from that speed.  Disabled, the drive will start from zero speed.

Resolution:
The ATV600 and ATV900 series both have a Catch on the Fly option.
ATV600 series:  this parameter is enabled by default
ATV900 series:  this parameter is disabled by default
Go to Complete Settings > Error/Warning Handling > Catch on the Fly > Catch on the Fly to adjust this parameter.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria