Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the Controller Inside Card for the ATV61/71 Drives?
Issue:
Part Number for the Controller Inside Card for the ATV61/71

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
The part number is VW3A3501. See attachment for a picture of the Controller Inside Card. This is a blank, programmable card. It does not come pre-programmed.

Schneider Electric Nigeria

Attachment(s)
Controller Inside card.png [235.19 KB]