{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is location of the heat sink fans and the fan power supplies on the High HP ATV660 and ATV960 enclosed drives?
Issue:
Heat sink fan and the fan power supplies location on the High HP ATV660 & ATV960 enclosed drives?

Product Line:
ATV660 ATV960 High HP enclosed drives only

Environment:
All

Cause:
Needs to locate the heat sink power supplies and the heat sink fan to troubleshoot.

Resolution:
Open the main Door of the enclosed ATV660 or ATV960 drive.
The 48vdc Fan control power supplies are mounted in the upper area.  Under 200KW drives use only one heat sink fan power supply.  200KW size and above uses two heat sink fan power supplies.
The heat sink fans are located in the bottom center of the drive.  Under 200KW size drives use one heat sink fan.  200KW size and above uses two heat sink fans.

locations

Example shows above 200KW frame size and it has both two fan power supplies and two heat sink fans.

Schneider Electric Nigeria