Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to find the weighing module PMESWT0100 DTM?

Article available in these languages: Spanish

Issue
I need to add the PMESWT0100 to my application but can not find it in the list of available DTMs.
Where to find the weighing module PMESWT0100 DTM?

Product Line

M580
X80

Environment
EcoStruxure Control Expert


Resolution

The weighing module PMESWT0100 DTM can be found on

  1. Control Expert installation

PME