Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
STB IO - why the STBACO1210 doesn't work if two sensors are connected with internal power supply mode
Question:
why the STBACO1210 doesn't work if two sensors are connected with internal power supply mode

Answer:
For STBACO1210,the two output channels are none isolated and you could choose one these options:
1, use external isolated DC power supply to each channel.

2. if use internal power supply, you can only use one channel to wire sensor (another channel as spare)