How can we help you today?

M580 - Is it possible to pack the memory of an M580 HSBY PLC online in run mode?

Question:
Is it possible to pack the memory of an M580 Hot Standby PLC online in run mode?

Answer:
Yes, M580 HSBY CPU can be packed online in run mode.
But if it is a M580 stand alone CPU, we recommend to use Unity Pro v10 or later, as on Unity v8.1 there is an issue when online pack a running M580 CPU.