Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Provide band range for Solo wireless pushbutton XB5R*, ZBRR*

Article available in these languages: French

ZigBee has 16 channels from 2405 to 2480 MHz. These frequencies are the center frequencies.
Each channel is separated by 5MHz but the channel bandwidth is 2 MHz
Our product is adjusted on the first channel 2405 MHz (channel 11). See attachment

To avoid any interference and keep a safety gap, the frequency band should be selected outside 2403,75 MHz - 2406,25 MHz

Schneider Electric Nigeria

Attachment(s)
Solo Zigbee frequency.png [62.58 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings