Issue:
Is it possible to change the color of a Vijeo Designer Toolchest images from the image library?
Product Line:
Vijeo Designer (all versions)
Resolution:
Today the easiest way to change the colors of any toolchest images from the image libraries is to use this procedure:
1) Drag the desired image on to your Vijeo Designer Panel
2) Select the image and then Copy (Ctrl + C)
3) Open Microsoft word and Paste (Ctrl + V)
4) Select the image in Microsoft word and then Copy (Ctrl + C)
5) Open Microsoft Paint and Paste (Ctrl + V)
6) Use the Color Filler to change the colors of the image
7) Once you are done, select the image and Copy/Paste into Microsoft Word again
8) Copy/Paste from Word to Vijeo Designer
9) In Vijeo Designer, enable the Anti-Alaising and set the transparent color to be the back ground color of the image.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Nigeria